When we run our 4.4_r1 test this test case does not run. Also, there is another holo test, android.host.holo and it doesn't even show up in the results.
The Freescale CTS test results do not mention this test case.
Anyone else having this experience?
Test Package Passed Failed Timed Out Not Executed Total Tests
android.holo 0 0 0 0 0
This test is officially removed from CTS for the time being. It will be put back at a future date. I removed it from the CTS.xml file to prevent the entry from messing up our test runs. We are using proprietary hardware based on SabreSD.
Hi James,
Which board are you using now?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------