CSI-MIPI for adv7280m,MIPI_CSI_PHY_STATE is always 0x200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI-MIPI for adv7280m,MIPI_CSI_PHY_STATE is always 0x200

1,323 Views
tukenan
Contributor II

my platform is imx6q.

1. when configure MIPI Camera Sensor to have all Tx lanes in PL-11 state,.the MIPI_CSI_PHY_STATE  is 0x610.

2. I switch on imx6 dphy before clearing CSITX_PWRDN, the MIPI_CSI_PHY_STATE  is always 0x200。 I think it may be 0x210。the step 6 is wrong for me. Who can help me?

pastedImage_1.png

Labels (1)
0 Kudos
6 Replies

1,023 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please look at suggestions on

i.MX6Q video capture issue with ADV7280-M 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,023 Views
tukenan
Contributor II

On what condition,the MIPI_CSI_PHY_STATE   is 200;

0 Kudos

1,023 Views
igorpadykov
NXP Employee
NXP Employee

check sect.40.6.6 General settings for all blocks (MIPI_CSI_PHY_STATE)

i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

0 Kudos

1,023 Views
tukenan
Contributor II
The problem has been solved. the pin for CLK is short 。 tks.

0 Kudos

1,023 Views
tukenan
Contributor II

396040146567318291.jpg

879273588071607370.jpg

the Clock and the data is in high speed mode。

0 Kudos

1,023 Views
tukenan
Contributor II

i know  the MIPI_CSI_PHY_STATE。But my adv7280m is from Low state mode (MIPI_CSI_PHY_STATE is 0x610 to high speed mode(  MIPI_CSI_PHY_STATE is 0x200),the bit4  and the  the bit 8 are not 1  。

0 Kudos