my platform is imx6q.
1. when configure MIPI Camera Sensor to have all Tx lanes in PL-11 state,.the MIPI_CSI_PHY_STATE is 0x610.
2. I switch on imx6 dphy before clearing CSITX_PWRDN, the MIPI_CSI_PHY_STATE is always 0x200。 I think it may be 0x210。the step 6 is wrong for me. Who can help me?
Hi
please look at suggestions on
i.MX6Q video capture issue with ADV7280-M
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
On what condition,the MIPI_CSI_PHY_STATE is 200;
check sect.40.6.6 General settings for all blocks (MIPI_CSI_PHY_STATE)
i.MX6DQ Reference Manual
the Clock and the data is in high speed mode。
i know the MIPI_CSI_PHY_STATE。But my adv7280m is from Low state mode (MIPI_CSI_PHY_STATE is 0x610 ) to high speed mode( MIPI_CSI_PHY_STATE is 0x200),the bit4 and the the bit 8 are not 1 。