CHANNEL_SELECT field when i.MX6 is set to eCSPI slave mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CHANNEL_SELECT field when i.MX6 is set to eCSPI slave mode.

Jump to solution
756 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 eCSPI.

I understand that CHANEL_SELECT field in ECSPIxCONREG register is set when i.MX6 is master mode and communicates with a external slave device.

Then, I want to confirm whether CHANNEL_SELECT field is also set in i.MX6DQ is eCSPI slave mode or not.

Would you let me know it?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
1 Solution
564 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The CHANNEL_SELECT field cannot be used to get the SS status.

Regards,

Yuri.

View solution in original post

0 Kudos
3 Replies
564 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 21.4.2 (Slave Mode) of the i.MX6 D/Q RM :

"In this configuration, Chip Select (SS) becomes an input signal, and is used to control

data transfers through the Shift register, as well as to load/store the data FIFO."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

564 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

Did you mean "we can confirm whether SS is input to i.MX6 or not by reading CHANNEL_MODE field"?

Or in slave mode, SS status is not affected to CHANNEL_MODE?

Best Regards,

Satoshi Shimoda

0 Kudos
565 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The CHANNEL_SELECT field cannot be used to get the SS status.

Regards,

Yuri.

0 Kudos