Hi,
We have got IMX6D custom designed board designed based on imx6Q reference board (Wandboard). in custom board we have 512 MB LPDDR2 where as reference board has 1GB/2GB DDR3 RAM.
Now we have connected mipi csi2 camera (Raspi camera (connector is also customized with 15 pin connector)).
When I am running the command for capturing image or video using avconv or gst-launch-1.0 then, image is not being captured.
When iam running the command as :
$ sudo avconv -f video4linux2 -r 30 -s 640x480 -i /dev/video0 out.avi (or)
$ sudo avconv -f video4linux2 -s 640x480 -i /dev/video0 -ss 0:0:2 -frames 1 test.jpg
then it is giving error as ioctl VIDIOC_REQBUFs
and "/dev/video0: No buffer space available"
Since ov5647 has on board crystal which generates 25 MHz clock, we are using mipi_dphy_clk = <0x28> is this correct or not?? in some cases, it is been given that mipi_dphy_clk = <0x14>??? which one we should use ????
When we are running this command, we are getting CSI_D0M,CSI_D0P, CSI_D1M, CSI_D1P correctly and laos getting 25 MHz clock from the crystal.
But we are not observing CSI_CLK0M (CN), CSI_CLK0P (CP) are not coming???? what could be the reason.
$gst-launch-1.0 v4l2src device="/dev/video0" num-buffers=1 ! video/x-bayer,width=640,height=480,framerate=1/1 ! bayer2rgb ! videoconvert ! jpegenc ! filesink location=sample_640_480.jpeg
then it is forming sample_640_480.jpeg file but it is not opening.
in all the above commands, when we are entering/running then led on the camera board is glowing and not when terminating the command, then led is going off.
Following are the findings:
1. camera sensor is being detecting in i2c by using i2c-tools (i2cdetect)
root@ubuntu:~# i2cdetect -y 2
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- UU -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
2.
root@ubuntu:~# lsmod
Module Size Used by
mxc_v4l2_capture 28532 1
ipu_bg_overlay_sdc 5401 1 mxc_v4l2_capture
ipu_still 2528 1 mxc_v4l2_capture
ipu_prp_enc 5943 1 mxc_v4l2_capture
ipu_csi_enc 3863 1 mxc_v4l2_capture
ipu_fg_overlay_sdc 6217 1 mxc_v4l2_capture
ov5647_camera_mipi 30906 0
which one we should use mipi_dphy_clock = <0x28> or mipi_dphy_clock = <0x14> if our camera sensor's clock is 25 MHz.
when iam dumping mipi csi2 regs by using devmem2 tool
[root@erez]# devmem 0x21dc000
0x3130302A
[root@erez]# devmem 0x21dc004
0x1
[root@erez]# devmem 0x21dc008
0x1
[root@erez]# devmem 0x21dc00c
0x1
[root@erez]# devmem 0x21dc010
0x1
[root@erez]# devmem 0x21dc014
0x200
[root@erez]# devmem 0x21dc018
0x0
[root@erez]# devmem 0x21dc020
0x00000000
[root@erez]# devmem 0x21dc024
0x0
[root@erez]# devmem 0x21dc02c
0x00000000
[root@erez]# devmem 0x21dc030
0x0
[root@erez]# devmem 0x21dc034
0x0
How resolve the issues????