CAN Driver iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Driver iMX6

3,460件の閲覧回数
djillaliredjrad
Contributor II


Hi,

I'm actually working with a CoM named Karo TX6DL who have iMX6DL chip with FlexCan module, I need to develop a driver for the CAN Bus but I don't know how to start, is there any library of functions like for microchip can controller ?

What's the reference of the FlexCan module, is it a SJA1000 ?

Thanks

0 件の賞賛
返信
1 返信

2,417件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Djillali

one can look at Sabre AI design, used TJA1041AT (sch-26662, p8)

Schematics (5)

Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards

Design files for Base Board (REV E)

Board Support Packages (38)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Driver description can be found in Chapter 37 FlexCAN Driver attached Linux Manual.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信