Dear all,
We have a question about Spread Spectrum of PLL2 of i.MX6UL.
Only PLL2(SystemPLL) supports Spread Spectrum.
We want to use this Spread Spectrum for a peripheral.
However, this PLL2 is used for MMDC module.
When DDR3L is used, may this Spread Spectrum cause any trouble?
In this case should PLL4 be chosen for MMDC?
May I have advice?
Best Regards,
Yuuki
Solved! Go to Solution.
Please refer to the following community thread:
https://community.nxp.com/message/376642
It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please refer to the following community thread:
https://community.nxp.com/message/376642
It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear all,
We want to apply Spread Spectrum for DDR3L to suppress the noise.
However, we must use PLL4 if Spread Spectrum adversely affects DDR3L.
May I have advice?
Best Regards,
Yuuki