CAMERA for android-passthrough of mipi-csi1 to android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAMERA for android-passthrough of mipi-csi1 to android

661 次查看
shabna_m
Contributor III

Hi,

My target is imx8quadmax mek.

I am running  linux -  imx-4.14.98-2.0.0_ga as dom0 and android-  imx-p9.0.0_2.1.0-auto-ga as domU on xen - imx-xen version 4.11 as per the virtualization guide.

I have tried to passthrough the mipi_csi1 camera to the android Domu, but failed.
I have got the following errors.
 

imx-lpi2c 58246000.i2c: can't get irq number

[   10.040053] Failed power operation on resource 322 sc_err 4

[   10.046105] imx8qm-pinctrl passthrough:iomuxc: pin_config_set op failed for pin 77

[   10.046141] ov5640_mipi_v3 5-003c: Error applying setting, reverse things back

[   10.046347] imx8qm-pinctrl passthrough:iomuxc: pin_config_set op failed for pin 77

[   10.046363] ov5640_mipi_v3 5-003c: Error applying setting, reverse things back

[   10.046382] ov5640_mipi_v3 5-003c: setup pinctrl failed

[   10.046404] ov5640_mipi_v3: probe of 5-003c failed with error -5

 

If someone has succeeded in passthrough the mipi_csi1 camera to the android domU,

Please help me to solve the issue.

 
 
0 项奖励
回复
1 回复

462 次查看
Jen2
Contributor I

Hello, have you succeeded?

0 项奖励
回复