Hi Folks,
I am working on secure u-boot on imx6, I wanted to use AES cryptography of CAAM driver, but in 2018 09 uboot source it only provides RSA cryptography.
NXP provides separate SDK for bare-board, I compiled that code with arm-linux-gnueabi tool chain but it gives data abort during loading CAAM bin at uboot console.
Please help me to how to use CAAM on imx6 uboot for AES encryption.
Thanks in advance.
Hello,
You can try using the MFG to load Your bare metal examples.
To load the test via MFG, add the following profile to the ucl2.xml :
<LIST name="DWLD_IN_SDP" desc="Download and execute a binary!">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="sdk_unit_test_caam.bin" >Loading U-boot</CMD>
<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>
</LIST>
Also, since all SDK sources are available, it is possible to build code
just for running under U-boot.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!