Build new kernel for imx6 ubuntu image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build new kernel for imx6 ubuntu image

2,436件の閲覧回数
asadlesani
Contributor I

Hi,

I'm going to build a kernel for Ubuntu 16.06 and kernel 4.1.15_2.0.0_ga.

I have a board based on iMX6-dl from Technexion company. They provided the access to their kernel and config and device tree files.

I use these steps to build kernel and add new modules (drivers) to the kernel such as ath9k for Atheros PCIe WiFi cards.

git clone https://github.com/TechNexion/linux.git && cd linux
export KERNEL_SRC=$PWD
export ARCH=arm
export CROSS_COMPILE=arm-linux-gnueabihf-

git checkout tn-imx_4.1.15_2.0.0_ga

make tn_imx_defconfig

make menuconfig

   add the drivers I need to the config file
make -j4 zImage modules imx6dl-edm1-cf-pmic_fairy.dtb

After these steps, the kernel is built without any error. In the log I see all the modules I've selected in menuconfig compiling without any error and I can see *.o files.

I also see *.ko files for the driver selected as "M" in menucconfig setting.

Once the built is finished I use these two command lines to add new kernel to the SD card that already flashed (and working) with the image the company providing with the same kernel and version of Ubuntu.

cp arch/arm/boot/zImage arch/arm/boot/dts/imx6dl-edm1-cf-pmic_fairy.dtb /media/user/74C5-8858/

make ARCH=arm modules_install INSTALL_MOD_PATH=/media/user/c8843fd8-cc57-4557-93a9-5fa0e596fa72/

When I use make module_install it just copies the *.ko drivers to the SD card.

I don't know how I can add other drivers that marked with " * " in menuconfig to the SD card such as "ath9k.o".

I'm new to these software things.

Any help for that? Am I missing anything?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,185件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Asad

in general recommended to rebuild all image with newly included drivers.

As this software was developed by third party, one can post on vendor support

Support - TechNexion 

or post this to meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
meta-freescale Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信