Build failure of secure firmware update using cst-3.1.0 tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build failure of secure firmware update using cst-3.1.0 tool

1,215 Views
vijith_g1
Contributor II

I am building an secure image for doing a secure firmware update using yocto linux. For that I have to use a signing tool. The signing tool cst tool which I downloaded from digi documents shows extract failure when I build using build command bitbake core-image-base.  I followed the instruction provided by digi for building secure image.  The instructions followed up are - copying the cst-3.1.0.tgz file in to download folder. Modify local.conf file as per digi documents for secure boot.

Please let me know whether I will get a supported cst tool or older versions of the cst tools. Please share the link for downloading older versions of the cst tools.

Please find the attached snap shot.

Labels (2)
0 Kudos
1 Reply

1,170 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Use the recent CST:

https://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL_NEW&location=null 

  Note, NXP recommendations how to build signed images are provided in U-boot documentation:
 

Regards,

Yuri.

0 Kudos