Hi all
I'm having the following error during build
Read error (Connection timed out) in headers.
Try linux-2.6.31-imx_10.10.00.bz2 from the GPP
http://bitshrine.org/gpp/linux-2.6.31-imx_10.10.00.bz2:
01:11:51 ERROR 404: Not Found.
Can't get: linux-2.6.31-imx_10.10.00.bz2 at ./ltib line 790.
I checked the given link and mentioned bz2 does not exists.
And idea why?
Thank you..
Hi Tugrul,
I have no idea where to get the patch as the kernel from the BSP is fullt functional.
However, to patch it you will have to change the .spec file.
Why not try the newer version of the kernel?
Regards,
Lee
What BSP is this? Looks like very old version (10.10 indicates it's from October 2010, and kernel version only 2.6.31). Get a newer version from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW