Bring up LVDS display in Android 14 for IMX8MPlus custo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bring up LVDS display in Android 14 for IMX8MPlus custo board

694 Views
abhiroopnray
Contributor III

Hi,

 

We are using a cutom IMX8MPLUS board and upgrading from #Android 13 to Android 1

We are using a specific display and I have the drivers. For Android 13, the customization in dts worked fine and the display was working. But same customization fro Android 14 is not working. 

 

The backlight is coming but it is coming like a white stripe. I have added the configurations following the datasheet same as in Android 13.

Can you tell me if there is any specific changes in ANdroid 14 from Android 13 for the LVDS display? Which specific file do I need to check for #Android 14

 

Thanks,

Abhiroop Nandi Ray 

0 Kudos
Reply
4 Replies

529 Views
subash_p
Contributor II

Hello @Bio_TICFSL ,

I encountered an issue where the LVDS display works correctly in Android 13 but fails to operate in Android 14, despite using the same DTS file for both versions.

0 Kudos
Reply

525 Views
abhiroopnray
Contributor III

Hi @subash_p ,

 

I have got the solution.

In Android 14, below lines need to be added in panel-simple.c file under drivers:

 

.bus_flags = DRM_BUS_FLAG_DE_HIGH,

 

Thanks,

Abhiroop Nandi Ray

0 Kudos
Reply

513 Views
subash_p
Contributor II
Hi @abhiroopnray,

This line was already added in my panel-simple.c file, I will mention the code below.


static const struct panel_desc rocktech_rk101ii01d_ct = {
.modes = &rocktech_rk101ii01d_ct_mode,
.bpc = 8,
.num_modes = 1,
.size = {
.width = 217,
.height = 136,
},
.delay = {
.prepare = 50,
.disable = 50,
},
.bus_flags = DRM_BUS_FLAG_DE_HIGH,
.bus_format = MEDIA_BUS_FMT_RGB888_1X7X4_SPWG,
.connector_type = DRM_MODE_CONNECTOR_LVDS,
};

Note : I'm using the rocktech,rk101ii01d-ct as compatible for my LVDS pannel

Thanks,
Subash Parthiban

670 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you change the dts in android 14 then it should works please create a case in our database.

 

Regards

0 Kudos
Reply