Boundary SABRE Lite i.MX6: is my SPI Flash broken or is U-Boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boundary SABRE Lite i.MX6: is my SPI Flash broken or is U-Boot?

Jump to solution
5,626 Views
louiskoziarz
Contributor II

Hi all,


I was hoping someone out there has some experience with the SPI Flash EEPROM on the new Boundary SABRE Lite board.

In the process of practicing with U-boot and the loader I've apparently messed up the SPI Flash on the board.  No big deal, so I'm rebooting in USB OTG mode and running U-Boot out of RAM.  When I try to run the 6q_upgrade script off of SD to reflash the board, it fails. 


It seems that spi_flash.c isn't getting the manufacturer code back from the Flash at the correct time.  I've recompiled with DEBUG and If I run the probe alone, I get the manufacturer code:

U-Boot > sf probe

SF: Got idcodes

00000000: bf 25 41 bf 25    .%A.%

SF: Detected SST25VF016B with page size 4 KiB, total 2 MiB

But if I run "sf probe 1" as the 6q_upgrade script likes to do, I get this:

U-Boot > sf probe 1

SF: Got idcodes

00000000: 00 00 00 00 00    .....

SF: Unsupported manufacturer 00

Failed to initialize SPI flash at 0:1

and just for kicks...

U-Boot > sf probe 0

SF: Got idcodes

00000000: 00 00 00 00 00    .....

SF: Unsupported manufacturer 00

Failed to initialize SPI flash at 0:0

Anyone have any ideas?

Thanks,

Louis Koziarz

Labels (1)
0 Kudos
Reply
1 Solution
2,271 Views
EricNelson
Senior Contributor II

Hi Louis,

Our latest, main-line based U-Boot introduced an incompatibility with respect to sf probe as discussed in this blog post.

Sorry I didn't catch this query. I'm not sure how I can subscribe to notifications of *SABRE Lite*|Nitrogen.


View solution in original post

0 Kudos
Reply
7 Replies
2,271 Views
luisgarcia
Contributor I

Hi Louis,

Reading your post, I have seen that you could add debugging options to u-boot. As a consequently, you get some messages about SPI FLASH memory (identifier, manufacturer, size). In my R+D group, I am working with a based-OMAPL137 custom board but it is almost similar to EVM board. At the booting, I have problems with the SPI recognition, because the SPI FLASH at the custom board is slightly different than the EVM SPI FLASH, I mean, I can see the uboot prompt, and type commands like printenv, setenv and so on but when I save these changes by means saveenv, following mesages are printed:

Failed to initialize SPI flash at 0:0

In order to solve that problem, I select the SPI FLASH 0 interface by means sf probe 0, but the result is the same...

For that reason, it would be very interesting know to compile the uboot with debugging options! I could see the same messages than you and fix mistakes!

Thanks in advance!

Regards

Luis

0 Kudos
Reply
2,271 Views
louiskoziarz
Contributor II

Luis,

I added my own printk calls inside of the SPI flash driver to get the information I wanted, then recompiled u-boot.  It's the only way to get the code to do what you want.

Good luck,

Louis

0 Kudos
Reply
2,271 Views
EricNelson
Senior Contributor II

Hi Luis,

This issue is fixed. Louis, please confirm.

We haven't seen any issues with SPI NOR on any boards since production began a long while ago.

The issue Louis was seeing stemmed from an incompatibility between different versions of U-Boot

Old (2009.08 version) had this syntax:

     U-Boot > sf probe 1

The new (2013 and later) has this syntax:

     U-Boot > sf probe

0 Kudos
Reply
2,271 Views
louiskoziarz
Contributor II

Eric,

Yes, the 2013 u-boot is working just fine with SPI flash now.  My problem stemmed from a newer bootloader with an older script.

- Louis

0 Kudos
Reply
2,271 Views
luisgarcia
Contributor I

Thanks Eric for your quick answer! I am going to try this procedure next monday. Respect to the debugging option at the uboot, any suggestion? Thanks in advance

Regards

Luis

0 Kudos
Reply
2,271 Views
louiskoziarz
Contributor II

Just to follow up some more, I've dug into the command/cmd_sf.c for the Boundary branch of U-Boot and I'm noticing that "sf probe" works correctly with no parameters because Chip Select (cs) is being set tot the default of CONFIG_SF_DEFAULT_CS (which is set in include/configs/nitrogen6x.h as it should be).

It's when the 0/1 parameter gets added to "sf probe" that cs gets set to 0 or 1 and the probe fails.  How is this working for others in the field?

0 Kudos
Reply
2,272 Views
EricNelson
Senior Contributor II

Hi Louis,

Our latest, main-line based U-Boot introduced an incompatibility with respect to sf probe as discussed in this blog post.

Sorry I didn't catch this query. I'm not sure how I can subscribe to notifications of *SABRE Lite*|Nitrogen.


0 Kudos
Reply