Boradcom BCM8950X BroadR-Reach Ethernet switch integration with i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boradcom BCM8950X BroadR-Reach Ethernet switch integration with i.MX6

2,429 次查看
shabeerbadarudh
Contributor IV

Hi All,

We are going to integrate BCM8950x  Broadcomm BroadR-Reach ethernet switch to i.MX6 host. Any one have idea about software configuration.

1. Any Linux drivers/Device tree details  are available for BCM8950x.

2. How do we test this switch   in Linux User space.

3. Any useful links / documents are available.

标签 (5)
0 项奖励
回复
2 回复数

1,014 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shabeer

BCM8950 is used on SABRE Auto CPU cards (switch card IMXAI2ETH-BRC)

Freescale's Audio Video Bridging Software for

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,015 次查看
shabeerbadarudh
Contributor IV

Hi Igor,

Thanks for your response!!

I have seen that page. But there is no download option. How can we get the AVB software? Is it propitiatory one?

Also we have seen the link https://community.freescale.com/docs/DOC-95578 explain about the AVB Demo setup in i.MX6 3.0.35 kernel.

Is the AVB support available in latest freescale BSP?(3.10.17 or 3.14)

Thanks,

Shabeer

0 项奖励
回复