hi,
Now I am using I.MX6UL development board named "i.MX6UltraLite Evaluation Kit (EVK)" . what i did is:
1: Install SDK_2.2_MCIM6UL on my PC.
2: Build one standalone elf executable file with demo IAR project in SDK folder “C:\nxp\SDK_2.2_MCIM6UL\boards\evkmcimx6ul\driver_examples\gpt\capture”.
2: press any key to stop auto-uboot, with uboot version "uboot-imx-imx_v2016.03_4.1.15_2.0.0_ga".
3: load elf file via command bootelf
=> fatload mmc 1:1 0x80800000 gpt_capture.out
reading gpt_capture.out
217948 bytes read in 35 ms (5.9 MiB/s)
4:Boot elf from memory.
=> bootelf 0x80800000
And my question is
1: Any idea why demo binary file execution is stuck? Assume application timer should start ticking.
2: How to disable interrupts initialized by U-boot? I mean how to diasble intterupts before bootelf command.
Thanks for the help in advance!
解決済! 解決策の投稿を見る。
Look at the following page. This page contains "Timer demo" example for using a CPM interrupt handler with the U-Boot code.
See also the following pages:
http://variwiki.com/index.php?title=Yocto_Customizing_U-Boot
https://boundarydevices.com/customizing-u-boot-on-i-mx/
https://www.quora.com/How-do-I-customize-the-U-boot-bootloader
https://community.nxp.com/thread/445938
http://xillybus.com/tutorials/uboot-hacking-howto-1
https://rocketboards.org/foswiki/Documentation/PreloaderUbootCustomization131
See the following document about u-boot customizing under Yocto:
Have a great day,
Pavel Chubakov
There are no recommendations from u-boot developers (www.denx.de) about similar u-boot changing.
It looks like that the following command sequence is needed.
Have a great day,
Pavel Chubakov
-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------
Look at the following page. This page contains "Timer demo" example for using a CPM interrupt handler with the U-Boot code.
See also the following pages:
http://variwiki.com/index.php?title=Yocto_Customizing_U-Boot
https://boundarydevices.com/customizing-u-boot-on-i-mx/
https://www.quora.com/How-do-I-customize-the-U-boot-bootloader
https://community.nxp.com/thread/445938
http://xillybus.com/tutorials/uboot-hacking-howto-1
https://rocketboards.org/foswiki/Documentation/PreloaderUbootCustomization131
See the following document about u-boot customizing under Yocto:
Have a great day,
Pavel Chubakov
Appreciate the links, it helpful for me. May I have one more asking. Could you share the guide/link about relocating vector table for RTOS in DDR by booting with uBoot.
Let me clarify myself, I am looking for the method to replace Uboot exception handler with my ROTS exception handlers .Thanks
The i.MX6 u-boot is not operating system.
Find the "Standalone HOWTO:" in u-boot README file.
This file is available using the following link:
https://github.com/u-boot/u-boot/blob/master/README
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi Pavel,
thanks for the help, checked. Booting standalone application are directly runnable in the environment
provided by U-Boot. But now I also need to install my own set of exception handlers, device drivers, set up the MMU, etc... like linux OS, and i also need the leverage HAB feature on I.MX6UL processor.
Could you give me some advice about below items:
1: Is customizing U-boot the fastest approach?Any other better approach for that?
2: If customizing U-boot is the fastest approach, could you help to share some guide/doc about that?
thanks
Can you use the bootelf to start an application? Could you share your findings?
One more input, after bootelf is called by Uboot, then connect IAR and start debugging, there is a warning in debug log "Tue Mar 12, 2019 09:22:19: The stack pointer for stack 'IRQ_STACK' (currently 0x00000013) is outside the stack range (0x800111C0 to 0x800112C0) "