Hi,
Iam building android 7.1.2 SabreAuto BSP for our board ,successfully flashed images into 16Gb microSD card using script fsl-sd-card-partition.shwhich is attached below.But when we powered on our board it boots up showing bootanimation and it get stuck showing boot image as shown below.
Complete debug log is attached along with this.
Console: switching to colour dummy device 80x30
watchdogd: started (interval 10, margin 20)!
EXT4-fs (mmcblk2p3): mounted filesystem with ordered data mode. Opts: barrier=1
EXT4-fs (mmcblk2p10): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p10): recovery complete
EXT4-fs (mmcblk2p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): recovery complete
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
EXT4-fs (mmcblk2p5): bad geometry: block count 393216 exceeds size of device (2048 blocks)
file system registered
using random self ethernet address
using random host ethernet address
zram0: detected capacity change from 0 to 314572800
logd.auditd: start
logd.klogd: 6305556999
Adding 307196k swap on /dev/block/zram0. Priority:-1 extents:1 across:307196k SS
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
binder: 254:254 transaction failed 29189, size 0-0
type=1400 audit(456.240:4): avc: denied { chown } for pid=256 comm="uim-sysfs" capability=0 scontext=u:r:hci_attach:s0 tcontext=u:r:hci_attach:s0 tclass=capability permissive=0
read descriptors
read strings
logd.daemon: reinit
sabreauto_6q:/ # android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
android_work: sent uevent USB_STATE=CONNECTED
configfs-gadget gadget: high-speed config #1: b
android_work: sent uevent USB_STATE=CONFIGURED
(stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
type=1400 audit(457.120:5): avc: denied { dac_override } for pid=256 comm="uim-sysfs" capability=1 scontext=u:r:hci_attach:s0 tcontext=u:r:hci_attach:s0 tclass=capability permissive=0
healthd: No battery devices found
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
(stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
type=1400 audit(459.280:6): avc: denied { dac_override } for pid=256 comm="uim-sysfs" capability=1 scontext=u:r:hci_attach:s0 tcontext=u:r:hci_attach:s0 tclass=capability permissive=0
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
(stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
type=1400 audit(461.440:7): avc: denied { dac_override } for pid=256 comm="uim-sysfs" capability=1 scontext=u:r:hci_attach:s0 tcontext=u:r:hci_attach:s0 tclass=capability permissive=0
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
(stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
type=1400 audit(463.600:8): avc: denied { dac_override } for pid=256 comm="uim-sysfs" capability=1 scontext=u:r:hci_attach:s0 tcontext=u:r:hci_attach:s0 tclass=capability permissive=0
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
(stk) : timed out waiting for ldisc to be un-installedBluetooth: st_register failed -22
random: crng init done
android_work: sent uevent USB_STATE=DISCONNECTED
init: write_file: Unable to write to '/config/usb_gadget/g1/UDC': Device or resource busy
android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
android_work: sent uevent USB_STATE=CONNECTED
configfs-gadget gadget: high-speed config #1: b
android_work: sent uevent USB_STATE=CONFIGURED
Can anyone help me to resolve this?Its urgent!
Note: I tried with MFG tools and gets otg works for loading u-boot and other binaries to ram . Its just mfgtool after "Jumping to OS" it stays at No Device connected"so tried using fsl-sd-card-partition.sh.
Thanks,
Richu
jimmychanigorpadykovqiusheng
jimmychannikolaos.pasaloukos@andromedadigital.com
解決済! 解決策の投稿を見る。
Hi igor,
Thanks for your prompt reply.
Actually the board was booting with out any issues with the same images in another sd card.Unfortunately i lost that sd card and brought another sd card.
working sd card log
new sd card log
both are part of logs of two sd cards(full log is attached along with this)
as you can see filesystem is not getting mounted in mmcblk2p5 in new sd card.
Is that flashed properly??
Please help me to resolve?
Thanks,
Richu
Hi Richu
one can try with other sd cards, preferably brand new.
Best regards
igor
Hi igor,
I finally got this work when execute commands in fsl-csrd-partition.sh manually.
Hi Richu,
I am also facing the same issue now, executing the script commands manually means do we need to partition the sd card manually using the gdisk command and copy the respective files to the sd card partitions?
Regards,
Parvathi.
Hi RICHU
one can try to run latest ddr test
i.MX6/7 DDR Stress Test Tool V3.00
and rebuild image with updated ddr calibration coefficients found from ddr test
in uboot ..freescale/mx7dsabresd/*.cfg file
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------