Boot i.MX8MN based custom board after FIELD_RETURN fuse was blown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot i.MX8MN based custom board after FIELD_RETURN fuse was blown

336 Views
thomasschaefer
Contributor III

Hi all,

I managed to blow FIELD_RETURN fuse on our (closed) i.MX8MN based custom board. Now I want to boot this board using an unsigned bootloader image file but no success. The SPL code starts and downloads remaining u-boot parts via BOOTROM API, but then boot messages stop:

U-Boot SPL 2022.04-00079-ga37bf36a47-dirty (Nov 02 2023 - 14:54:37 +0000)
Normal Boot
WDT: Started watchdog@30280000 with servicing (60s timeout)
Trying to boot from BOOTROM
Find img info 0x&48025a00, size 932
Need continue download 1024
Download 719920, Total size 721456
ROM download finished OK

As can be seen, the unsigned bootloader is able to start on the FIELD_RETURN fused board, but then stops when ATF firmware is going to be executed.

I have enabled the CONFIG_ARMV8_SPL_EXCEPTION_VECTORS setting to workaround the ROM serror issue with ATF firmware (see https://www.mail-archive.com/u-boot@lists.denx.de/msg376429.html).

I can boot that bootloader image to prompt using an unlocked device of that same board:

 

U-Boot SPL 2022.04-00079-ga37bf36a47-dirty (Nov 02 2023 - 14:54:37 +0000)
Normal Boot
WDT: Started watchdog@30280000 with servicing (60s timeout)
Trying to boot from BOOTROM
Find img info 0x&48025a00, size 932
Need continue download 1024
Download 719920, Total size 721456
ROM download finished OK
NOTICE: BL31: v2.2(release):rel_imx_5.4.47_2.2.0-0-gc949a888e-dirty
NOTICE: BL31: Built : 11:10:34, Dec 9 2022


U-Boot 2022.04-00079-ga37bf36a47-dirty (Nov 02 2023 - 14:54:37 +0000)

CPU: Freescale i.MX8MNano UltraLite Quad rev1.0 at 1200 MHz
Reset cause: POR
Model:
DRAM: 1 GiB
Core: 67 devices, 19 uclasses, devicetree: separate
WDT: Started watchdog@30280000 with servicing (60s timeout)
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
In: serial@30a60000
Out: serial@30a60000
Err: serial@30a60000

BuildInfo:
- ATF c949a88

Net: eth0: ethernet@30be0000
Hit any key to stop autoboot: 0
u-boot=>

 

What am I missing to make the (unsigned) bootloader boot to prompt on the FIELD_RETURN enabled board?

Best regards,

Thomas

 

 

Labels (1)
0 Kudos
3 Replies

299 Views
thomasschaefer
Contributor III

Hi Harvey,

the intention is to allow end users in some case to disable secure boot in order to comply with open source licenses.

As said, we have been able to blow FIELD_RETURN fuse on our board, but we are not able to boot unsigned bootloader image (the same is true when trying a signed image) to u-boot prompt.

Do you have any ideas why boot process stops after SPL execution?

 

Best regards,

Thomas

0 Kudos

267 Views
thomasschaefer
Contributor III

Any new ideas/comments/suggestions to this topic?

0 Kudos

303 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @thomasschaefer 

Field Return: This level is intended for the parts returned from the shipped products.

 

Best regards

Harvey

0 Kudos