Hello,
I am designing with iMX6D.
I will use the IPU1_CSI0 & IPU2_CSI1 at same time.
So. EIM pins will be used for IPU2_CSI1. (8bit Data = EIM_A17~A24(IPU2_CSI1_DATA12~19)), (PIXCLK=EIM_A16),(HSYNC=EIM_DA11),(VSYNC=EIM_DA12)
EIM pins are also used "Boot config".
I can configure EIM pins at power on.
But I can define these pins at software reset.
Do I need to set "boot config" when software reset.
Thanks.
解決済! 解決策の投稿を見る。
Hi John
yes it is necessary to set "boot config" using software reset.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi John
yes it is necessary to set "boot config" using software reset.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks your answer.
Is the pin that I can know "software reset"?
Thanks.
there is no pin for "software reset"
~igor