Boot Contact Pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot Contact Pins

759件の閲覧回数
DaviddeBethel
Contributor I

Hi Folks,

 

Can anybody give me any advice on the best way to set up the boot contact pins on the IMX257?

 

I wish to know if they all MUST be connected or can I connect the ones corresponding to NAND Flash (which I am using) to high, whilst leaving the non-required pins as no-connect.  I know this is classed as floating and may not be a good idea.

 

Else, I must use pull down resistors, but I worry that this may affect the use of the peripherals associated with these pins, such as CSPI2.

 

Any advice would be most gratefully received

 

ddB

ラベル(1)
0 件の賞賛
2 返答(返信)

683件の閲覧回数
OmarPighi
Contributor I
yes this is interesting, but is there any tool to read/blow fuses status for prototipe and production?
0 件の賞賛

683件の閲覧回数
Frias
Contributor V

Hello David,

 

Instead of using the external IO you can use the e-fuses to determine how the SoC boots.

 

Best Regards,

Renato Frias 

0 件の賞賛