Hi
We have custom board based on mx6qsabresd board design
We use Temple run apk to test the board performance
Few of our boards are rebooting when the application runs
We suspected the DDR can be an issue,So we did a DDR test
that also passed
What can be the reason
Attaching the DDR configuration file
Uboot version : 2014 : 04
Regards
Himanshu
Original Attachment has been moved to: mx6q_4x_mt41j128.cfg.zip
已解决! 转到解答。
Hello Igor
This issue is resolved ,the issue was with our watchdog configuration
it was not configured properly in the devicetree imx6q-sabresd-ldo.dts
Thanks for you support
Regards
Himanshu
Hi himanshu
this may be caused by hardware and one can recheck
recommendations in
HW Design Checking List for i.MX6DQSDL
one can try following experiments to determine if it is a hardware PCB issue
(power voltages ripples):
hand solder 22uF capacitors directly under center of chip. Solder on top of the 0402 chips.
have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor
Below is the scenario
The issue is not observed in all the hardwares
in 40% of the hardware issue is occurring
Also in those 40% of hardware in which issue occurs if we put previous version of software
Android JB, issue is not reproduced
After further analysis In Issue Hardwares we found
1.40% of hardware in which issue occurs issue observed when ever temperature reaches above 60-62 Celsius
2.In the rest 60% of hardwares even if temperature reaches above 60-62 Celsius device works properly it doesn't reboots
Regards
Himanshu
Hello Igor
Below are the set working frequencies
cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq/scaling_available_frequencies
396000 792000 996000
cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
396000
the cpu frequency is set as minimum only
With memory are we referring to DDR frequency ?
Regards
Himanshu
Hi Igor
Sure,will check that
Just in addition to the observation in the issue boards
The board reboots not just on running Temple Run apk
Infact we tried heating the processor(using heat gun) without running any application
and observed the board reset (watchdog) at the temperature range (62-66)
Lower than this temperature range board doesn't reset even if we run the Temple run apk
and keep on cooling the processor using the cooling gun .
But in similar hardware setup when we tried the older version JB,the board didn't reset
at all(neither by running Temple run apk nor by the heating processor by external means)
So this eliminates the issue on the hardware side.
Just wanted to let you know so that we can focus on the right direction
Regards
Himanshu
Hi Himanshu
you can also check if all latest patches are applied,
Also try to reproduce this issue on Sabre reference board, this will point direction:
if this relates to custom hardware board or this is just software issue.
~igor
Hi Igor
Please find the register dump of DDR register for Lollipop uboot
and Jellybean uboot ,I found few differences w.r.t few register
Jellybean Uboot
HIM:DDR 0x021b08b8 value read = 690000
HIM:DDR 0x021b48b8 value read = 6c0000
HIM:REG 0x020e0010 value read = 0
HIM:REG 0x020e0018 value read = 22222222
HIM:REG 0x020e001C value read = 22222222
HIM:REG 0x020c4060 value read = a0001
HIM:REG 0x020c4068 value read = ffffffff
HIM:REG 0x020c406c value read = ffffffff
HIM:REG 0x020c4070 value read = ffffcfff
HIM:REG 0x020c4074 value read = ffff3fcf
HIM:REG 0x020c4078 value read = ffffffff
HIM:REG 0x020c407c value read = ffffffff
HIM:REG 0x020c4080 value read = ffffffff
Lollipop uboot
HIM:DDR 0x021b08b8 value read = 640000
HIM:DDR 0x021b48b8 value read = 670000
HIM:REG 0x020e0010 value read = f00000cf
HIM:REG 0x020e0018 value read = 7f007f
HIM:REG 0x020e001C value read = 7f007f
HIM:REG 0x020c4060 value read = fb
HIM:REG 0x020c4068 value read = c03f3f
HIM:REG 0x020c406c value read = 30fc03
HIM:REG 0x020c4070 value read = fffc033
HIM:REG 0x020c4074 value read = 3ff0f003
HIM:REG 0x020c4078 value read = fff300
HIM:REG 0x020c407c value read = f0000f3
HIM:REG 0x020c4080 value read = 3ff
Note: we dont see device reboot issue with JB
Can these register differences can cause the issue in Lollipop
Also Iam not sure where the issue is ,Is it at kernel Level or at Uboot level
Regards
Himanshu
Hi Himanshu
suggest to run ddr test and set ddr settings according to
its results
i.MX6/7 DDR Stress Test Tool V2.40
~igor
Hi Igor
tried this ,the issue still persist
seems like the issue is at the kernel level
As at uboot level i tried running DDR test and externalyy heated the processor
was unable to see the board rebooting
You have any idea on what in the kernel level can affect rebooting of the tool
at certain temperature
Regards
Himanshu
Hi Himanshu
if you think that this is kernel bug, please
try to reproduce this on Sabre NXP/FSL reference board.
If this issue will not appear on reference board, then
problem in custom board.
~igor
Hello Igor
This issue is resolved ,the issue was with our watchdog configuration
it was not configured properly in the devicetree imx6q-sabresd-ldo.dts
Thanks for you support
Regards
Himanshu
I Igor
I booted my device with buildroot (uramdisk) (using same rest of LP images)
and i am not able to see the issue of device rebooting at that particular temp.
which means issue might be related to graphics
Do you have any clue on this
Regards
Himanshu