Bluetooth on Android startup failing with D-BUS No Such Adapter error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth on Android startup failing with D-BUS No Such Adapter error

Jump to solution
3,477 Views
bdp42
Contributor IV

I'm attempting to get Bluetooth working on an iMX53-based platform running i.MX Android R10.2. Android version is 2.3.3.

I've got it to the stage where I can manually perform a hciattach and this seems to work OK but when I attempt to start Bluetooth via the Android GUI it fails. Here is a snippet from logcat and the failure appears to be Dbus-related (No Such Adapter)

I've looked around various forums but have not made too much progress.

Any ideas as to the cause of the problem?

Thanks

Bruno

D/BluetoothService( 2084): Bluetooth state 10 -> 11

V/BluetoothEventRedirector( 2206): Received andrBDP rfkill set power 0

oid.bluetooth.adapter.action.STATE_CHANGED

I/bluedroid( 2084): Starting hciattach daemon

I/bluedroid( 2084): Starting bluetoothd deamon

E/BluetoothEventLoop.cpp( 2084): get_adapter_path: D-Bus error: org.bluez.Error.NoSuchAdapter (No such adapter)

E/BluetoothEventLoop.cpp( 2084): failure setting up Event Loop!

E/BluetoothEventLoop.cpp( 2084): get_adapter_path: D-Bus error: org.bluez.Error.NoSuchAdapter (No such adapter)

E/BluetoothEventLoop.cpp( 2084): failure setting up Event Loop!

D/BluetoothService( 2084): bt EnableThread giving up

I/bluedroid( 2084): Stopping bluetoothd deamon

BDP rfkill set power 1

I/bluedroid( 2084): Stopping hciattach deamon

D/BluetoothService( 2084): Bluetooth state 11 -> 10

V/BluetoothEventRedirector( 2206): Received android.bluetooth.adapter.action.STATE_CHANGED

Here's what I see when I do a manual hciattach and hciconfig

# hciattach -s 115200 /dev/ttymxc4 texas 3000000 flow

[ATH_INFO] (external/bluetooth/bluez/

tools/hciattach.c) <init_uart>: Serial port is opened
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Port settings is gotten
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Port settings is set
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Initial baud rate is set
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Break is sent
Found a Texas Instruments' chip!
Firmware file : /system/lib/firmware/ti/TIInit_7.6.15.bts
Sending script to serial device
Loaded BTS script version 1
texas: changing baud rate to 3000000, flow control to 1
CCCCCCCCCCCCCCCCCCCCWRCSCCCCCWRCCWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRCCWRWRWRWRWRCCCCCWRWRWRWRWRWRWRWRWRCCCWRCCCCCCCCCCCCCCCWRCCWRCCCWRCCCCWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRWRCCCCCCWRCCWRCCWRCWRCCCCCCWRCCCC
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: u->init is loaded
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Actual baud rate is set
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Line discipline is set
[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: Ioctl device is set

Added device hci0
Sending script to bluetooth socket

[ATH_INFO] (external/bluetooth/bluez/tools/hciattach.c) <init_uart>: u->post is loaded
Device setup complete

# hciconfig
hci0:   Type: BR/EDR  Bus: UART
        BD Address: 34:B1:F7:97:8E:CE  ACL MTU: 1021:4  SCO MTU: 180:4
        UP RUNNING
        RX bytes:352 acl:0 sco:0 events:10 errors:0
        TX bytes:45 acl:0 sco:0 commands:10 errors:0

Here's the relevant piece from the init.rc file

# Prepare for bluetooth
    chmod 665 /sys/class/rfkill/rfkill0/state
    chown bluetooth bluetooth /sys/class/rfkill/rfkill0/state
    write /sys/class/rfkill/rfkill0/state 0

chmod 0660 /dev/ttymxc4

chown bluetooth bluetooth /dev/ttymxc4

service dbus /system/bin/dbus-daemon --system --nofork

    socket dbus stream 660 bluetooth bluetooth

    user bluetooth

    group bluetooth net_bt_admin

service bluetoothd /system/bin/bluetoothd -n

    socket bluetooth stream 660 bluetooth bluetooth

    socket dbus_bluetooth stream 660 bluetooth bluetooth

    # init.rc does not yet support applying capabilities, so run as root and

    # let bluetoothd drop uid to bluetooth with the right linux capabilities

    group bluetooth net_bt_admin misc

    disabled

service hfag /system/bin/sdptool add --channel=10 HFAG

    user bluetooth

    group bluetooth net_bt_admin

    disabled

    oneshot

service hsag /system/bin/sdptool add --channel=11 HSAG

    user bluetooth

    group bluetooth net_bt_admin

    disabled

    oneshot

service opush /system/bin/sdptool add --channel=12 OPUSH

    user bluetooth

    group bluetooth net_bt_admin

    disabled

    oneshot

service pbap /system/bin/sdptool add --channel=19 PBAP

    user bluetooth

    group bluetooth net_bt_admin

    disabled

    oneshot

service hciattach /system/bin/hciattach -n -s 115200 /dev/ttymxc4 texas 3000000 flow

    user bluetooth

    group bluetooth net_bt_admin

    disabled

Labels (2)
0 Kudos
Reply
1 Solution
1,756 Views
bdp42
Contributor IV

The problem was eventually found to be caused by hciattach being unable to open the hci0 device because it lacked NET_ADMIN capabilities. I changed the user from 'bluetooth' to 'root' in init.rc where the hciattach service is defined.

There may be another way to fix this but this did work and I did see an init.rc for the wireless device (TI WL127XX) with user set to root. This may be of help to someone else.

View solution in original post

0 Kudos
Reply
2 Replies
1,756 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

this error my be caused by improper/incompatible bluez version, please check links below

Qualcomm Bluetooth D-Bus problem - Development - RootzWiki

platform_external_bluez/utils/doc/manager-api.txt at master · android/platform_external_bluez · GitH...

Also it may be recommended to post it on specialized bluez forums.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,757 Views
bdp42
Contributor IV

The problem was eventually found to be caused by hciattach being unable to open the hci0 device because it lacked NET_ADMIN capabilities. I changed the user from 'bluetooth' to 'root' in init.rc where the hciattach service is defined.

There may be another way to fix this but this did work and I did see an init.rc for the wireless device (TI WL127XX) with user set to root. This may be of help to someone else.

0 Kudos
Reply