Bluetooth and Wifi connectivity in imx6qsabreauto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth and Wifi connectivity in imx6qsabreauto

672 Views
saseendranathvs
Contributor I

Hi,

On the bottom part of IMX6qSabreAuto board, there is a Wi-Fi ® SD Card Slot and BT Module Connector. 

I want to know which Wifi SD card and which BT module is most suitable and is easily available for this board. Which devices are supported ?.How to make it working ?

I have seen that Broadcom BCM4339 is supported. But I couldnt find any devices or daughter boards for imx6qsabreauto board. Kindly suggest some.

I am using linux OS

0 Kudos
Reply
1 Reply

577 Views
igorpadykov
NXP Employee
NXP Employee

Hi Saseendranath

please refer to

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

also after registering vendor of modules provide additional documents for connection

and usage like below

wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_linux.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply