Bluedroid on Android kitkat 4.4.3 and i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluedroid on Android kitkat 4.4.3 and i.MX6SL

763 次查看
mutyalaraoneela
Contributor III

Hi All,

Platform : IMX6SL

Bluedroid on Android kitkat 4.4.3.

Can you please help me I am struck at this point not able to move forward.

D/BluetoothAdapterState(  704):  CURRENT_STATE=PENDING, MESSAGE = ENABLE_TIMEOUT, isTurningOn=true, isTurningOff=false
E/BluetoothAdapterState(  704): Error enabling Bluetooth
D/BluetoothAdapterProperties(  704): Setting state to 10
I/BluetoothAdapterState(  704): Bluetooth adapter state changed: 11-> 10
D/BluetoothAdapterService(  704): Broadcasting updateAdapterState() to 1 receivers.

what's wrong with this..... Not getting any idea. Please help me.....

Thanks and regards,

MutyalaRao.

0 项奖励
回复
2 回复数

533 次查看
isaacavila
NXP Employee
NXP Employee

Hi Mutyalarao,

I recommend you to ask this question in IMX community (i.MX Community ) due this is related to IMX6SL.

In i.MX community, you can look for related topics or create a new discussion.

Best regards,

Isaac

0 项奖励
回复

533 次查看
mutyalaraoneela
Contributor III

Hi all,

  I am glad to inform you that the above issue which I have posted earlier got resolved, but I have another issue while data transfer.

    After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :

   File not Received

   File : sample.jpg

   Reason : Storage issue

  Please suggest me how to proceed further???

Thanks and Regards,

Mutyala Rao.

0 项奖励
回复