Hi,
I'm working with imx6ull based board. In my system, I'm using an SPI device.
SPI device driver used is an iio driver.
I found the bits per word in the communication as 8 bpw, and required length is 32bpw.
I configured spi-> bits_per_word as 32, but the system hangs on booting.
How to change the burst length?
Hi mathew
in general changing spi-> bits_per_word should not affect boot,
one can try to find place in code where it hangs using
AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------