BSP for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP for IMX6

Jump to solution
1,310 Views
hjpark71
Contributor III

Hi NXP,

I have a question..

Do you provide IMX6 board's BSP through Yocto project only  or provides through the general distribution channel ?

Recently, I have started S/W development on IMX6 boards and saw many documents using Yocto for IMX6 BSP.

for me, Yocto is very complex and not easy to handle it..

My target is to make very tiny kernel and rootfs for IMX6 and doesn't need everything from Yocto.

If you can provide me your general BSP(toolchain, kernel, uboot, rootfs) for IMX6, it will be very appreciated..

Thanks a lot..

Best Regards,

HJ

Labels (1)
0 Kudos
1 Solution
694 Views
saurabh206
Senior Contributor III

Hi Hj

Yocto is simple.

Rootfs and tool chain you can build using Yocto.

After that you can work independently for kernel and u-boot.

Following are the links from where you can download the u-boot and kernel source code.

u-boot.git - Automotive U-Boot Tree

linux-2.6-imx.git - Freescale i.MX Linux Tree

Thanks

Saurabh

View solution in original post

0 Kudos
2 Replies
694 Views
edison_fernande
Contributor III

Hi HJ,

If you want an easy to use BSP you can go here: RidgeRun , we have SDKs for several iMX6 eval boards and you can get a free evaluation version of any of our SDKs. Depending on your needs this would be enough or a good starting point and you can always reach us for any help you need.

Here is also the downloads page:

RidgeRun

And here you can find some useful information:

Category:IMX6 - RidgeRun Developer Connection

Regards,

Edison

0 Kudos
695 Views
saurabh206
Senior Contributor III

Hi Hj

Yocto is simple.

Rootfs and tool chain you can build using Yocto.

After that you can work independently for kernel and u-boot.

Following are the links from where you can download the u-boot and kernel source code.

u-boot.git - Automotive U-Boot Tree

linux-2.6-imx.git - Freescale i.MX Linux Tree

Thanks

Saurabh

0 Kudos