BSP for 4.1.15_1.0.0_ga login issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP for 4.1.15_1.0.0_ga login issue

713件の閲覧回数
lixuhui112
Contributor I

my Yocto Project is "fsl-yocto-imx-4.1.15_1.0.0"

my board is MCIMX6Q-sdb

I use bitbake core-image-minimal 

boot from SD ,download iamge tftp ,and use  nfs mount  file system ,everything is normal Except login

such as :  it can not login

pastedImage_0.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

525件の閲覧回数
Yuri
NXP Employee
NXP Employee

Also, please use "no_root_squash" option.

~Yuri.

0 件の賞賛
返信

525件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  root account has some specifics for NFS.

Root Access On NFS

permissions - Why can't root on one machine change nfs mounted content from another machine? - Unix ...

  Also, please use "i.MX_Linux_User's_Guide.pdf" in documentation package

for more details how to use NFS.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

525件の閲覧回数
lixuhui112
Contributor I

HI Yuri Muhin

       Thank you for your reply!

       I can use NFS mount filesystem ,but I can not  use root account login the board

0 件の賞賛
返信