BOOT OPTIONS ON iMX8M mini board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOOT OPTIONS ON iMX8M mini board

1,819件の閲覧回数
giacomobiancala
Contributor I

Hi,

I need a clarification about boot options on iMX8M mini processor.

I am developing a custom Board based on iMX8M mini. I have 2 BOOT options.

- eMMC (on uSDHC3). In this case NVCC_NAND = 1,8V

- uSD port (on uSDHC2). In this case NVCC_SD2 =3.3V

I also have NVCC_SD1=3,3V.

I have some doubts about BOOT_CFG[6:4] and BOOT_CFG[3:1].

BOOT_MODE referred to 1,8V and the other pins referred to 3,3V. Is it ok?

Is it correct attached table?

Thanks,

Giacomo

ラベル(1)
0 件の賞賛
8 返答(返信)

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

You can share your schematic on mrudang.shelat@volansystech.com. If you want you can remove the project name and customer name etc.

Regards,

Mrudang

0 件の賞賛

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

As per our email conversation, this thread is closed.

Kindly acknowledge and assign new ticket if you have any other query.

Regards,

Mrudang  

0 件の賞賛

1,571件の閲覧回数
giacomobiancala
Contributor I

Hi Mrudang,

Sorry for my late answer. Finally I have defined boot options and all seems clear. If you have a private contact I can Share electrical schematics.

Regards

Giacomo

0 件の賞賛

1,571件の閲覧回数
giacomobiancala
Contributor I

Hi Mrudang,

Thank you for your answer.

I changed voltages domains.

In conclusion I have all voltage domains NVCC_xxxx at 3.3V (excepted NVCC_NAND for eMMC). 

Moreover uSDHC for SD CARD is uSDHC1 instead of uSDHC2.

Did you read my attached BOOT pinout tables?

Regards,

Giacomo

0 件の賞賛

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Kindly share your schematic for CPU, eMMC, SDIO and Boot section.

This will help me to provide a complete solution of your query.

Regards,

Mrudang

0 件の賞賛

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Any update?

Regards,

Mrudang

0 件の賞賛

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Kindly provide Boot_Mode domain pin supply voltage. It should be the same power compatible with all BOOT_MODE and JTAG and Test_MODE. 

What do you mean by other pins? Kindly provide the details.

If it is the same as a compatible supply for BOOT_MODE and NVCC_JTAG, then it is good to go ahead. 

Regards,

Mrudang

0 件の賞賛

1,571件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi  Giacomo,

Any updates here?

Regards,

Mrudang

0 件の賞賛