In the IMX6SDLRM, table 8-4 on page 392 says:
BOOT_MODE[1:0] | BT_FUSE_SEL Value | Boot Options Controlled By |
---|---|---|
00 | 0 | eFUSEs |
00 | 1 | eFUSEs |
01 | 0 | GPIO pins |
01 | 1 | eFUSEs |
10 | 0 | GPIO pins |
10 | 1 | eFUSEs |
What I take from this is that regardless of the boot mode, eFUSES should be used if either of the two conditions are true:
- the boot mode is 00 (Boot from Fuses)
- the BT_FUSE_SEL fuse has been set
Thus, I *should* be able to boot from fuses on a board by setting the BOOT_MODE to 00 and leaving BT_FUSE_SEL intact, however I am not finding this to be the case in the test boards I am working on. I have jumper pins for the BOOT_MODE, and have set BOOT_CFG1 to 0x00005068 (booting from MMC on SD3), however until I burn BT_FUSE_SEL, I *cannot* boot the board, even in BOOT_MODE 00. Could someone explain what I'm missing? I really need the ability to go back and forth between boot modes 00 and 01...
Thank you in advance for your help!
In Boot_From_Fuses mode (00b), BT_FUSE_SEL is used by the boot ROM to control the boot flow. With BT_FUSE_SEL=0, the boot ROM goes straight into the serial downloader. With BT_FUSE_SEL=1, the boot ROM attempts to boot from the boot device selected in the boot config fuses.
The intent is to allow a board to be built with a blank i.MX6(x) and blank memory. With the board strapped to boot from fuses mode, the device will go straight into serial downloader mode the first time it is booted. Production equipment would then use this mode to load an image into memory and burn BT_FUSE_SEL. The next time the board boots, it will run the image.
Note that in serial downloader mode (10b), BT_FUSE_SEL is not used.
This behavior is documented in section 8.2.3 of the i.MX6 S/DL reference manual.
Gary Segal wrote:
In Boot_From_Fuses mode (00b), BT_FUSE_SEL is used by the boot ROM to control the boot flow. With BT_FUSE_SEL=0, the boot ROM goes straight into the serial downloader. With BT_FUSE_SEL=1, the boot ROM attempts to boot from the boot device selected in the boot config fuses.
The intent is to allow a board to be built with a blank i.MX6(x) and blank memory. With the board strapped to boot from fuses mode, the device will go straight into serial downloader mode the first time it is booted. Production equipment would then use this mode to load an image into memory and burn BT_FUSE_SEL. The next time the board boots, it will run the image.
Note that in serial downloader mode (10b), BT_FUSE_SEL is not used.
This behavior is documented in section 8.2.3 of the i.MX6 S/DL reference manual.
What about Internal Boot mode (01b) ? According to the table, BT_FUSE_SEL is used in all three modes (00b, 01b, and 10b). I'm trying to work out how to get the ability to switch back and forth from one boot medium to another using a button at power-on to switch from 00b to 01b. If I *must* burn BT_FUSE_SEL to use Boot From Fuses mode (00b), then that prohibits use of Internal Boot mode (01b) if BT_FUSE_SEL overrides the GPIO pins. This is the situation that lead me to attempting to boot in 00b without burning BT_FUSE_SEL...
If you want to change the boot device, select internal boot mode (BOOT_MODE=01b) and use GPIO overrides by keeping BT_FUSE_SEL at 0 (don't burn it). This is how the Freescale Sabre manages boot device selection.
Enjoy.
I understand the confusion in this regard, unfortunately as Gary Segal mentioned you would need to blow the BT_FUSE_SEL value in order to boot accordingly to the eFuse options, otherwise you would jump into serial download mode when Booting from Fuses (00b).
You may have multiple booting options (as in Freescale’s SABRE board for example) but it’s usually the final booting configuration what’s blown into the fuses in manufacturing. In this stage it’s desirable to lock the booting options to the wanted setting.
Hi,
Send your post to imx community (e.g. i.MX Community ) to get it visible for active members.
Saurabh