BOOT_CFG_LOCK Documentation Clarification on i.MX 6ULL PRM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BOOT_CFG_LOCK Documentation Clarification on i.MX 6ULL PRM

Jump to solution
1,640 Views
JohnKlug
Senior Contributor I

This is page 226 of i.MX6 ULL Applications Processor Reference Manual, Rev 1, 11/2017.  What does "X" mean?  Normally it is don't care in most usages.  But 1x and x1 are contradictory it seems.  In the settings column of 5-9, it does not say which of the two bits is being set.

boot_cfg_lock_1.pngboot_cfg_lock_2.png

0 Kudos
Reply
1 Solution
1,587 Views
Yuri
NXP Employee
NXP Employee

@JohnKlug 
Hello,

   OP means Override Protection.

OP still enable to burn fuses but prevent manipulation at run time (using OCOTP).
Once the device is in production, the fuses have to be burned. Then OP+WP should
lock them.

WP only, would still enable a run time fuse manipulation.

 

Regards,
Yuri.

View solution in original post

4 Replies
1,591 Views
JohnKlug
Senior Contributor I

I assume OP means open, and WP means write protect, so what does a fuse setting of 11 mean?  That is why this does not make any sense to me.  I assume 00 means open or not write protected.

0 Kudos
Reply
1,617 Views
JohnKlug
Senior Contributor I

So what does it mean if both fuses are set?  Can it be open and write protected at the same time?

0 Kudos
Reply
1,588 Views
Yuri
NXP Employee
NXP Employee

@JohnKlug 
Hello,

   OP means Override Protection.

OP still enable to burn fuses but prevent manipulation at run time (using OCOTP).
Once the device is in production, the fuses have to be burned. Then OP+WP should
lock them.

WP only, would still enable a run time fuse manipulation.

 

Regards,
Yuri.

1,621 Views
Yuri
NXP Employee
NXP Employee

@JohnKlug 
Hello,

  in the Lock Fusemap, for BOOT_CFG_LOCK, bit 3 is responsible for the OP, 
bit 2 is responsible for the WP.

Regards,
Yuri.

0 Kudos
Reply