Hi all,
We are using imx_"3.14.38_6qp_ga yocto fido" bsp in our custom board.
Here sometimes we are facing issue in audio recording. while recording its showing below print.
"overrun!!! (at least 1.921 ms long)".
command used to record is "arecord -d 10 test.wav". This issue is present only in AC97 audio codec.
Could anybody help me to solve this.
Thanks in advance.
Regards,
Yashavantha
解決済! 解決策の投稿を見る。
Hello,
I an afraid the issue concerns with Linux file system performance.
You may try using SD card of class 10 or /dev/shm node for RAMFS for relatively
short files.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I an afraid the issue concerns with Linux file system performance.
You may try using SD card of class 10 or /dev/shm node for RAMFS for relatively
short files.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------