Audio issue with IMX6 board (max98357a)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Audio issue with IMX6 board (max98357a)

跳至解决方案
4,371 次查看
vladzouth
Contributor II

Hello NXP Community,

I'am working on a custom board based on IMX6 Solo processor and TX6S-8035 module, trying to play audio with MAX98357a codec. I just start leaning how works the device-tree I implement a simple-audio-card on the 4.1.15 linux kernel and use the following DTS as suggested in i.MX6 and MA98357a with simple-audio-card:

    codec: max98357a@0 {
        compatible = "maxim,max98357a";
        #sound-dai-cells = <0>;
    };

    sound {
        compatible = "simple-audio-card";
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ssi1>;
        simple-audio-card,name = "TI3 Audio";
        simple-audio-card,format = "i2s";
        simple-audio-card,widgets = "Speaker", "Speakers";
        simple-audio-card,routing = "Speakers", "Speaker";
        simple-audio-card,bitclock-master = <&cpu_dai>;
        simple-audio-card,frame-master = <&cpu_dai>;
        cpu_dai: simple-audio-card,cpu {
            sound-dai = <&ssi1>;
            system-clock-frequency = <883200>;
            dai-tdm-slot-num = <2>;
            dai-tdm-slot-width = <16>;
        };
        codec_dai: simple-audio-card,codec {
            sound-dai = <&codec>;
        };
    };
&audmux {
status = "okay";
// Note: 'ssi1' (node of first SSI) corresponds to '_SSI0' below.
ssi1 {
     fsl,audmux-port = <MX31_AUDMUX_PORT1_SSI0>;
     fsl,port-config = <
           0x00000000
           IMX_AUDMUX_V2_PDCR_RXDSEL(MX31_AUDMUX_PORT3_SSI_PINS_3)
           >;
       };

aud3 {
      fsl,audmux-port = <MX31_AUDMUX_PORT3_SSI_PINS_3>;
      fsl,port-config = <
          (IMX_AUDMUX_V2_PTCR_TFSDIR |
          IMX_AUDMUX_V2_PTCR_TFSEL(MX31_AUDMUX_PORT1_SSI0) |
          IMX_AUDMUX_V2_PTCR_TCLKDIR |
          IMX_AUDMUX_V2_PTCR_TCSEL(MX31_AUDMUX_PORT1_SSI0))
          IMX_AUDMUX_V2_PDCR_RXDSEL(MX31_AUDMUX_PORT1_SSI0)
          >;
     };
};

&ssi1 {
      fsl,mode = "i2s-master";
      assigned-clocks = <&clks IMX6QDL_CLK_SSI1_SEL>, <&clks IMX6QDL_CLK_SSI1>;
      assigned-clock-parents = <&clks IMX6QDL_CLK_PLL4_AUDIO_DIV>;
      assigned-clock-rates = <0>, <49152000>; // 48kHz on SSI1 clock
      status = "okay";    
};
The MAX98357a codec is connected to SSI1. The soundcard is detected by ALSA. But when i try to play an audio file, i have nothing out on the speaker and there is no I2S signal on the SSI1 pin. Does somebody has any idea for this issue.
Thanks.
Best Regard!
Souleymane
0 项奖励
回复
1 解答
3,502 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Souleymane

statement "MAX98357a codec is connected to SSI1" is not fully correct as

SSI ports are connected through AUDMUX and described in Table 81. AUDMUX Port Allocatio,

Figure 16-1. AUDMUX Block Diagram i.MX6SDL Datasheet and i.MX6SDL Reference Manual

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 
http://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf

So one can check TX6S-8035 module schematic to find what AUDMUX port used for codec

connection.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,502 次查看
brobin
Contributor I

I had some trouble getting the sound card (MA98357a codec with the simple-audio-card) to work with a recent revision of the imx6q (i.MX 6 Quad), so I am sharing my solution, posted here: linux device driver - Audio issue with IMX6 board (max98357a codec) - Stack Overflow 

0 项奖励
回复
3,503 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Souleymane

statement "MAX98357a codec is connected to SSI1" is not fully correct as

SSI ports are connected through AUDMUX and described in Table 81. AUDMUX Port Allocatio,

Figure 16-1. AUDMUX Block Diagram i.MX6SDL Datasheet and i.MX6SDL Reference Manual

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 
http://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf

So one can check TX6S-8035 module schematic to find what AUDMUX port used for codec

connection.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复