Hi All,
We are facing strange issue of loosing audio after ~10 hrs of playback.
Platform:: We have customized platform of SabreSD i.MX 6Q.
Audio Source connected on port-5 of AUDMUX as MASTER using I2S. Port-1 connected SSI-1. Hence, audio received from AudioSource chip -> PORT-5 -> PORT-1 -> SSI-1.
Audio Codec (playback) connected on Port-6 of AUDMUX as SLAVE using I2S. Port-2 connected SSI-2. Hence, audio playback through SSI-2 -> PORT-2 -> PORT-6 -> Audio Codec chip
Existing audio driver for recording path was SSI-1 -> MEMORY. Means one DMA channel setup for DMA_FROM_DEVICE.
We have introduced ASRC in between Recording path (SSI-1 -> ASRC -> MEMORY). So, we have setup two DMA channel; one for SSI-1 -> ASRC i.e. DMA_DEV_TO_DEV & second for ASRC -> MEMORY i.e. DMA_FROM_DEVICE at driver level.
We reference existing playback source code of DMA Channel setup for DMA_DEV_TO_DEV.
Bus width for above channels are DMA_SLAVE_BUSWIDTH_2_BYTES.
Modified clock source of ssi1_clk, ssi2_clk & ssi3_clk to pll4_audio_main_clk in clock.c file.
Now, in our android applicatin we receive recording samples using AudioRecord object & play those sample using AudioTrack. This task done in only one thread at application side.
Result:
After above setup we are able to play recoreded content for approx ~10 hrs. but after that we receive error: "Unvalid SDMA MODE" & audio lost.
As per this log, it seems that DMA channel for DMA_DEV_TO_DEV (SSI-1 -> ASRC) met with an error.We try to read reg value of SDMAARM_EVTERR (Ref pg. no-4871:: 55.20.10 -DMA Request Error Register (SDMAARM_EVTERR) i.MX 6Q RM).
Which suggest that error bit set for above channel; this probably means there is an overflow of data for that channel.
But we could not identify how its possible.
Can anybody help me out to find where we made mistake in setup of DMA channel ? What is the probable reason for above scenario ?
For everybody reference, i am attaching patch here-with.
Please go through it & give comments upon it.
-Ankit.
Original Attachment has been moved to: asrc_V1_for_fsl_community.zip
Hi NXP..
I've also same issue. We use slave mode SSI0. SSI1 output and SSI1 input.
We play music continuously throughout SSI0 output ( 48kHz, 16bit LSB mode and use ASRC) .
System doesn't play anything and is holding after printing out log "Unvalid SDMA mode".
I think that this issue is not resolved from NXP. this issue is critical issue for stability.
Jongho/Ankit,
I know this is an old thread, but I am wondering if the following U-Boot patch could help on this issue?
Hi,
Lei Ge
Thanks for reply..
But Attached patched is already there in our kernel.
We have already allocated memory using dma_alloc_noncahced.
static int sdma_request_channel(struct sdma_channel *sdmac)
{
struct sdma_engine *sdma = sdmac->sdma;
int channel = sdmac->channel;
int ret = -EBUSY;
sdmac->bd = dma_alloc_noncached(NULL, PAGE_SIZE, &sdmac->bd_phys, GFP_KERNEL);
if (!sdmac->bd) {
ret = -ENOMEM;
goto out;
}
Thanks
Saurabh
leige-b42127, do you think the problem of ankitpatel, it is related to use one chip for Capture and another for Playback?. I would said that I2S in slave mode should be able to handle both. An idea that I have is to remove one of the chips, starting for the capture, and just playback from a file save in memory. If the error it is still present this would indicate that is something with the memory instead of a problem with the Audio interface.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lei Ge,
There is no issue when we play normal audio file from memory, there is no audio lost till unlimited time..
As we mentioned earlier in post that we got error of "Unvalid SDMA MODE" when there was Audio lost.
"" As per this log, it seems that DMA channel for DMA_DEV_TO_DEV (SSI-1 -> ASRC) met with an error.We try to read reg value of SDMAARM_EVTERR (Ref pg. no-4871:: 55.20.10 -DMA Request Error Register (SDMAARM_EVTERR) i.MX 6Q RM). Which suggest that error bit set for above channel; this probably means there is an overflow of data for that channel."
If SDMA met with an overflow of data, it automatically STOP the dma channel ??
-Ankit.
If overflow happend, module will not send new request to SDMA, except there is bus error while SDMA transfer data, SDMA script will stop the channel
can you try to adjust the brustsize of the SDMA between SSI and ASRC ?
Hi Lei Ge,
Currently, these are the value set:
1. Value set to '4' in receive FIFO Watermark (RFWM0) field in the SSI FIFO Control/Status Register (SFCSR).
2. bus width=DMA_SLAVE_BUSWIDTH_2_BYTES
3. Parameters, Lower WML (0-7 bit) & Higher WML (16-23 bit), each set to '8' in p_2_p (r7 INFO). Means current burstsize is '8' for p2p channel.
Following experiment i am going to do for modifying burstsize of SDMA between SSI and ASRC.
I will set value '8' in receive FIFO Watermark (RFWM0) field in the SSI FIFO Control/Status Register (SFCSR).
I will set Parameters, Lower WML (0-7 bit) & Higher WML (16-23 bit), to '16'. Hence, burstsize will become 16.
Is it correnct?.
-Ankit.
hi, how do you store the music file? do you have enough memory to store the recorded music file(10 hours long), if every 10 hours this issue happens, is this a not enough store memory issue?
Hi Lei Ge,
The value of 'sdmac->mode' is 'SDMA_MODE_P2P'. When i setup the P2P channel (SSI->ASRC), mode value set to 'SDMA_MODE_P2P'.
On interrupt received (because of 'overflow'), i print value of reg 'SDMA_H_EVTERR' & channel details:
//code is below
default:
spin_lock_irqsave(&sdma->irq_reg_lock, flag);
stat = readl_relaxed(sdma->regs + SDMA_H_EVTERR);
spin_unlock_irqrestore(&sdma->irq_reg_lock, flag);
pr_err("SDMA_H_EVTERR: %x, ch:%d, id:%d", stat, sdmac->channel, sdmac->chan.chan_id);
pr_err("Unvalid SDMA MODE!\n");
// Log print is:
SDMA_H_EVTERR: 4, ch:2, id:1
Unvalid SDMA MODE!
When i setup the P2P channel, i took the value of channel & its id:
//Log print is:
###ASRC RECORD: P2P dma channel ID:1 CONFIGURED! ASRC RX ReqID:37, SSI RX ReqID: 17
We are not storing audio recorded data in music file.
In our android application we receive recording samples using 'AudioRecord' object & play those sample using 'AudioTrack'. This task done in only one thread at application side.
-Ankit.
Hi Ankit, which kernel are you using. I am trying to put together something similar (spdif to ssi over asrc using p2p dma) and I wonder with which kernel you are seeing this "Invalid SDMA mode". Thanks