Asymmetric multiprocessing with two A7 cores of i.MX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Asymmetric multiprocessing with two A7 cores of i.MX7

555 Views
j-p-b-20
Contributor I

Hello,

I am working with i.MX7 that has a two A7 cores and a M4 core. In the first one is running Linux and the second one bare-metal. Now, I need to separated the two A7 cores and run a bare-metal (independent of M4) in a A7 and Linux in other A7. The M4 still would run her bare-metal. 

Can I do this?

I had seen an example with i.MX6. It has two A9 core and in one core is running Linux and in the other core is running FreeRTOS, but i don't know if i can do something similar with the i.MX7

Thanks.

Labels (2)
0 Kudos
1 Reply

455 Views
igorpadykov
NXP Employee
NXP Employee

Hi Josu

yes the same approach can be implemented for i.MX7,

may be useful to check linux documentaion on nxp i.mx software page

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos