Ask L2.6.35_11.09.01_ER_source_bundle.tar.gz installation package for iMX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ask L2.6.35_11.09.01_ER_source_bundle.tar.gz installation package for iMX53

461件の閲覧回数
Mike3333
Contributor I

Hello, Engineers of NXP,

     Could you please provide me with the following documents? I can't find them now。

    1. L2.6.35_11.09.01_ER_source_bundle.tar.gz

    2. i.MX53_START_Linux_BSP_UserGuide.pdf

    3. i.MX53_START_Linux_BSP_Release_Note.pdf

    If you really can't find them, please provide me with the following installation package:

    L2.6.35_11.01.00_ER_source_bundle.tar.gz

    L2.6.35_11.05.01_ER_source_bundle.tar.gz

 

0 件の賞賛
返信
0 返答(返信)