Andrtoid 13 Build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Andrtoid 13 Build error

1,260 Views
Beginner1122
Contributor II

I am trying to build android 13 image for INVENSOM-8MM NXP iMX SOM board by following the android user guide but facing the build errors kindly help me in building the image successfully, When I run this command it don't build the image and the all the images files such as uboot.img,root ,system,u-boot-imx8mm.imx:files are not created in this directory /out/target/product 


rmt@rmt-pc:/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build$ ./imx-make.sh -j4 2>&1 | tee build-log.txt
make: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build' rm -rf /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh mkdir -p /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_COLLECTION if [ -n "0" ]; then \ echo 'export ROLLBACK_INDEX_IN_FIT=0' > /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ echo 'export ROLLBACK_INDEX_IN_CONTAINER=0' >> /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ else \ echo 'export ROLLBACK_INDEX_IN_FIT=' > /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ echo 'export ROLLBACK_INDEX_IN_CONTAINER=' >> /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ fi; \ if [ "" = "true" ]; then \ echo 'export TEE_COMPRESS_ENABLE=' >> /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ else \ echo 'export TEE_COMPRESS_ENABLE=' >> /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ/ubootenv.sh; \ fi if [ "" = "true" ]; then \ dd if=/dev/zero of=vendor/nxp-opensource/imx-mkimage/iMX8M/dek_blob_fit_dummy.bin bs=96 count=1 && sync; \ else \ rm -f vendor/nxp-opensource/imx-mkimage/iMX8M/dek_blob_fit_dummy.bin; \ fi Merging KERNEL config srcs: /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/imx_v8_android_defconfig /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/device/nxp/imx8m/invsom_8mm/android_addition_defconfig Building arm64 2022.04 U-Boot ... . /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/device/nxp/imx8m/invsom_8mm/AndroidUboot.sh; \ build_m4_image Using /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/imx_v8_android_defconfig as base Merging /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/device/nxp/imx8m/invsom_8mm/android_addition_defconfig make[1]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx' make[2]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ' Value of CONFIG_USB_SERIAL_OPTION is redefined by fragment /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/device/nxp/imx8m/invsom_8mm/android_addition_defconfig: Previous value: CONFIG_USB_SERIAL_OPTION=m New value: CONFIG_USB_SERIAL_OPTION=y make[1]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/kernel_imx' make[2]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/KERNEL_OBJ' GEN Makefile CLEAN scripts/basic CLEAN scripts/kconfig CLEAN scripts/dtc CLEAN spl/u-boot.cfg CLEAN include/generated/env.in u-boot.cfg u-boot.cfg.configs CLEAN include/config include/generated spl include/asm CLEAN .config .config.old include/autoconf.mk include/autoconf.mk.dep include/config.h include/asm make[2]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ' make[1]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx' make[1]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx' make[2]: Entering directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ' HOSTCC scripts/basic/fixdep GEN Makefile HOSTCC scripts/kconfig/conf.o YACC scripts/kconfig/zconf.tab.c LEX scripts/kconfig/zconf.lex.c HOSTCC scripts/kconfig/zconf.tab.o ./.tmp.config.5XkC1hRYjA:1542:warning: override: reassigning to symbol PPP_SYNC_TTY # # configuration written to .config # make[2]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/KERNEL_OBJ' make[1]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/kernel_imx' HOSTLD scripts/kconfig/conf # # configuration written to .config # make[2]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/obj/UBOOT_OBJ' make[1]: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx' Value requested for CONFIG_INPHI_PHY not in final .config Requested value: CONFIG_INPHI_PHY=y Actual value: /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx is not clean, please run 'make mrproper' in the '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx' directory. make[2]: *** [/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/vendor/nxp-opensource/uboot-imx/Makefile:1928: prepare3] Error 1 make[2]: *** Waiting for unfinished jobs.... make[1]: *** [Makefile:177: sub-make] Error 2 make: *** [/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/device/nxp/common/build/uboot.mk:137: /media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build/out/target/product/invsom_8mm/u-boot.imx] Error 1 make: *** Waiting for unfinished jobs.... Value requested for CONFIG_WLAN_VENDOR_NXP not in final .config Requested value: CONFIG_WLAN_VENDOR_NXP=n Actual value: Value requested for CONFIG_MXMWIFIEX not in final .config Requested value: CONFIG_MXMWIFIEX=m Actual value: Value requested for CONFIG_CLD_HL_SDIO_CORE not in final .config Requested value: CONFIG_CLD_HL_SDIO_CORE=y Actual value: Value requested for CONFIG_PLIP not in final .config Requested value: CONFIG_PLIP=y Actual value: Value requested for CONFIG_PPP_SYNC_TTY not in final .config Requested value: CONFIG_PPP_SYNC_TTY=y CONFIG_PPP_SYNC_TTY=y Actual value: CONFIG_PPP_SYNC_TTY=y Value requested for CONFIG_PPPOATM not in final .config Requested value: CONFIG_PPPOATM=y Actual value: Value requested for CONFIG_PPP_SYNC_TTY not in final .config Requested value: CONFIG_PPP_SYNC_TTY=y CONFIG_PPP_SYNC_TTY=y Actual value: CONFIG_PPP_SYNC_TTY=y Value requested for CONFIG_REGULATOR_DUMMY not in final .config Requested value: CONFIG_REGULATOR_DUMMY=y Actual value: Value requested for CONFIG_EARLY_PRINTK not in final .config Requested value: CONFIG_EARLY_PRINTK=y Actual value: Value requested for CONFIG_DEBUG_PRINTK not in final .config Requested value: CONFIG_DEBUG_PRINTK=y Actual value: Value requested for CONFIG_DEBUG_LL not in final .config Requested value: CONFIG_DEBUG_LL=y Actual value: Value requested for CONFIG_DRM_LONTIUM_LT8912 not in final .config Requested value: CONFIG_DRM_LONTIUM_LT8912=y Actual value: make: Leaving directory '/media/rmt/Harddrive/imx-android-13.0.0_1.0.0/android_build'

0 Kudos
Reply
1 Reply

1,240 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It looks like it missed some package to build android, but android 13 works as usual with a NXP board you have to see with your vendor.

regards

0 Kudos
Reply