[Android] System reboot when running GFXBench 3.0.16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Android] System reboot when running GFXBench 3.0.16

1,586 次查看
charleshuang
Senior Contributor II

Hi Freescale,

 

We encounter a problem when we run GFXBench 3.0.16 benchmark.

The test steps are as below.

1. Install GFXBench 3.0.16.apk

2. Select the "Render Quality" test item and run

3. Then, system may reboot automatically.

    PS. It may not reboot every time. If not, you can try to run the test again.

 

You can find the APK file in the attachment.

Please help to investigate this issue.

Thank you.

 

Best regards,

Daniel

Original Attachment has been moved to: GFXBench_3.0.16.apk.zip

标签 (3)
0 项奖励
回复
2 回复数

1,148 次查看
danielhung
Contributor III

Hi Freescale,

Update more information for you.

It seems to die in Render Quality test item due to out of memory.

This issue happens on both JB4.3 & KK4.4, and it also can be found on Freescale demo board with both JB4.3 & KK 4.4 images.

The reproduce rate is about 50% or more.

Best regards,

Daniel

0 项奖励
回复

1,148 次查看
danielhung
Contributor III

If you cannot observe this issue, just try to run the test twice continuously.

I find it will be very easy to reproduce.


In addition, when this issue happens, the screen may become corrupted. Then, it reboot suddenly.

I can also reproduce it on Android JB 4.2.2.

0 项奖励
回复