Android 9 image burn at sdcard IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 9 image burn at sdcard IMX6

ソリューションへジャンプ
551件の閲覧回数
leonardoprates
Contributor III

I have Android 9 running on IMX6 board with SDCARD. I can burn the sdcard using a script provided by NXP at out/target/product/sabresd/. It's works, no problem. At Android 6 I can copy the result SDCARD using a sdcard duplicator machine or DD at Linux without any problem. Now in Android 9 sdcard, that uses GPT, this copy doesn't work, even with linux dd raw copy. Anyone have a idea of reason for a raw copied SDCARD doesn't work (boot)? Are there some kind of verification or anything else that can explain this?

Thank you,

Leonardo

0 件の賞賛
返信
1 解決策
537件の閲覧回数
leonardoprates
Contributor III

Answer my own question:

Android uses GPT and the table is at last 512 bytes of the card. The script write this table exactly at this position of the card. If I try to reproduce the sdcard, it will work only if the cards are exaclty the same size. If not, the table will not stay in the last 512 positions and device will not boot.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
538件の閲覧回数
leonardoprates
Contributor III

Answer my own question:

Android uses GPT and the table is at last 512 bytes of the card. The script write this table exactly at this position of the card. If I try to reproduce the sdcard, it will work only if the cards are exaclty the same size. If not, the table will not stay in the last 512 positions and device will not boot.

0 件の賞賛
返信
545件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You could download the Android 9 documentation from here

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

There is Android User's Guide. Please read the Chapter 5 "Programming Images" for more information.

 

0 件の賞賛
返信