Android 7 Bluethooth Stack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 7 Bluethooth Stack

1,129 次查看
jith
Contributor II

Hi,

Which is the Bluetooth stack used in Android 7?

Is it support Bluetooth 5?

标签 (1)
2 回复数

847 次查看
jith
Contributor II

Thank you so much

0 项奖励

847 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jith

as Android 7 is based on L4.1.15 kernel one can refer to

sect.55.3.3 Bluetooth Stack attached Linux Manual

Android N7.1.1_1.0.0 Release Announcement 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------