Android 5 and screen 1280x480

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 5 and screen 1280x480

754 次查看
yuribocharov
Contributor I

Hello!

I am working with SABRE AI board (imx6 quad) and trying to install Android.

I have installed android_L5.0.0_1.0.0-ga_tools.tar.gz  on sd card.

I want to use display with 1280x480 resolution.

It works but cuts bottom  part of image.

I have configured in this way:

=> setenv bootargs console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,1280x480M@60,if=RGB666 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc3 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled

=> saveenv

Saving Environment to MMC...

Writing to MMC(1)... done

How I can do it to show correctly?

标签 (2)
0 项奖励
回复
1 回复

510 次查看
igorpadykov
NXP Employee
NXP Employee

HI Yuri

please look at example

How to change SABRE-SD screen resolution in LOLLIPOP(5.0.0?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复