Hi Experts,
The IMX 6 SL EVK Android 5.1.1.2 build freezes after bootup. Then the kernel hangs after some times.
Kindly find the logs below,
PM: suspend entry 1970-01-01 00:01:19.686132634 UTC
PM: Syncing filesystems ... done.
Freezing user space processes ...
PM: Wakeup pending, aborting suspend
last active wakeup source: eventpoll
Freezing of tasks aborted after 0.007 seconds (36 tasks refusing to freeze, wq_busy=0):
Restarting tasks ... done.
PM: suspend exit 1970-01-01 00:01:19.742020884 UTC
PM: suspend entry 1970-01-01 00:01:20.075762301 UTC
PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.001 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
Suspending console(s) (use no_console_suspend to debug
Hi Dan,
Thanks for the reply.
There is no error observed during the compilation process. But when the USB OTG cable remains plugged in then the above issues doesn't comes. Here how to disable the Suspend/resume in the Freescale AOSP ?
Lyf
Hi Lyf,
Sorry for late reply. When the android system boot up, and then go to sleep mode, when you insert other device such as USB flash disk, mouse or keyboard by USB OTG the system will awake. So here you can go to the setting options on your android system, to set the display time. It will be OK.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------