Analog Camera with M4 Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Analog Camera with M4 Core

2,083 Views
burakdinc
Contributor I

Hi,
I'm working on IMX6 SoloX. When the Board is energized I need to control an Analog Camera with M4 as soon as possible (before Android initialize completed). For M4 Core, I'm using "FreeRTOS IMX6 SoloX". I couldn't find any C library or driver about VADC, CSI, LCDIF and LVDS.
I guess modifying and implementing linux driver files for my application could be an option. Is it possible to modify linux drivers for M4 Core? or should I write all drivers for M4?

If modifying linux drivers for M4 is appropriate, could you please tell me which files should i implement?

Labels (1)
0 Kudos
Reply
1 Reply

1,975 Views
igorpadykov
NXP Employee
NXP Employee

Hi burak

please find attached Linux Manual and Porting Guide with description

of all nxp linux drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply