Adding NodeJS to L5.4.24_2.1.0 (Ubuntu 18.04 LTS)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding NodeJS to L5.4.24_2.1.0 (Ubuntu 18.04 LTS)

688 次查看
prashant_chopad
Contributor II

Hello All,

I have iMX8M Mini EVK.

I did setup a Yocto toolchain for version L5.4.24_2.1.0 on my Ubuntu 18.04 LTS system.

I did successfully "bitbake imx-image-multimedia"

Need to add support for nodejs.

Would you please refer a link to do that?

How to include latest nodejs?

Regards,

Prashant

 

0 项奖励
回复
1 回复

675 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello prashant,

You may add a layer to an image by adding following line to the conf/local.conf file inside the build directory, and then baking the image.
IMAGE_INSTALL_append = “ nodejs”

Whenever you want to see which packages are available on the BSP you can run:
bitbake -s

 

Regards

 

0 项奖励
回复