I am new to both Linux and to the i.MX6 SoloX. I am able to generate executables that run on Linux on the A9-core of the i.MX6 SoloX SABRE-SD. However, I seem to be having trouble trying to accesses memory directly (via pointers) per the System Memory Map specified in Table 2-1 of the reference manual. Is Linux using a virtual memory map? Can you please provide a procedure to be able to read/write to raw memory?
With this procedure I would like to be able to access the OCRAM, M4 TCM, and memory mapped CPU registers so that my program running on the Linux A9 core can interact/control the M4 core.
Solved! Go to Solution.
For direct memory access Linux provides special node /dev/mem, which is used
by such tools as devmem. Really in our BSP there is the similar utility memtool
in /unit_tests directory. Basically You may look at memtool sources. Note, accesses
to non-supported address regions (hardcoded in /dev/mem driver) may cause system
issues.
Supported registers may be shown using the next command
$ /unit_tests/memtool .
or
$ /unit_tests/memtool *
For help
$ /unit_tests/memtool
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
For direct memory access Linux provides special node /dev/mem, which is used
by such tools as devmem. Really in our BSP there is the similar utility memtool
in /unit_tests directory. Basically You may look at memtool sources. Note, accesses
to non-supported address regions (hardcoded in /dev/mem driver) may cause system
issues.
Supported registers may be shown using the next command
$ /unit_tests/memtool .
or
$ /unit_tests/memtool *
For help
$ /unit_tests/memtool
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------