Hi, i am using SABRE-SDP, Linux 3.10.53 and SD card boot.
Uboot, Kernel and file systems are all in SD Card.
After boot process, it is shown in console when typing '# cat /proc/partitions'.
31 0 32 mtdblock0
179 0 3872256 mmcblk2 <-- 4G byte SD Card
179 1 8192 mmcblk2p1
179 2 991232 mmcblk2p2
179 8 31344 mmcblk3
My question is that where is eMMC. I can not find eMMC, it is on my board but not displayed.
How can I mount eMMC to my linux system?
已解决! 转到解答。
root@imx6qsabresd:~# ls /dev/mmcblk*
/dev/mmcblk2 /dev/mmcblk2p1 /dev/mmcblk2p2 /dev/mmcblk3
There are only mmcblk2 and mmcblk3.
root@imx6qsabresd:~# fdisk /dev/mmcblk3 -l
Disk /dev/mmcblk3: 30.6 MiB, 32096256 bytes, 62688 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
mmcblk3 is 32096256 bytes. SABRE has 8GB eMMC, so i think it is not eMMC.