The System Controller firmware API does not have support to access the I2C bus between SCU and the PMIC in iMX8qm. We need to be able to send commands to the PMIC from the Linux user space running in the APs, possibly via RPC call. We're especially interested in functions like
status_t i2c_write(..); and i2c_read(..) provided by the SCFW source code.
Is there a reasonable workaround that doesn't require kernel changes and adding extra commands to the SCU API?#
Hi All,
Did anyone able to modify SCU I2C registers from AP with Linux, Even I want to perform write on address 0x4a (AMUX_SEL) to get appropriate pmic internal sensor value on AMUX_OUT of PMIC chip, running
"pmic.w 0x09 0x4a 0x2e" on SCU UART works fine but I want make this work from AP with Linux. Any suggestion would be really helpful.
access may be performed with function dynamic_pmic_register_access() -
allows access to individual registers of the PMIC, described in
sect.16.14.3.6 dynamic_pmic_register_access() sc_fw_port.pdf document
included in SCFW Porting Kit
Best regards
igor
Hi mehdi
access to pmic with i2c is supported by scfw, please refer to attached ../mx8qm_mek/board.c
file from SCFW Porting Kit
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your reply. This doesn't however address our problem. We know the I2C communication with PMICs is managed and supported by the SCU firmware (in fsl_pmic.h file). We are interested in calling the I2C read/write routines from the application processors running Linux, somehow using the SCFW API and via an RPC call.
>We are interested in calling the I2C read/write routines from the application
>processors running Linux, somehow using the SCFW API and via an RPC call.
one can refer to sect.2.2 System Controller attached Linux Manual and Porting
Guide included in SCFW Porting Kit
In particular one can pay attention to below
https://community.nxp.com/docs/DOC-340335
Best regards
igor