About unintentional voltage application before powered on the i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About unintentional voltage application before powered on the i.MX6DQ.

跳至解决方案
1,465 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello.

The below voltage may occur to the I2C SDA line by external connected device before powered on the i.MX6DQ.

Voltage : 2.0V

Apply Time : 20us

(Board : Custom board)

In this case, is there possibility to destroy i.MX6DQ?

We hope that i.MX6 has the overvoltage protection.

(If it is possible, how many voltage is it possible to endure in i.MX6?)

Best Regards,

Keita

标签 (2)
0 项奖励
回复
1 解答
1,341 次查看
jamesbone
NXP TechSupport
NXP TechSupport

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

ANSWER: Yes, all the GPIO Type Pads had an overvoltage protection

[Q2]

Is there limitation on the time of voltage applied?

ANSWER. Yes there are but the value it is not available in our datasheet, so it is not validated, I apologize for the inconvenience.

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

ANSWER.  If you we are talking about the I2C pad, it is different from the GPIO pad, nevertheless it is in the same pin, so I do not see any problem applying the 2.0v for 20ms


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,341 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Keita,

We do not see a problem of the i.Mx6DQ get destroy for applying this 2.0v  for 20ms to the board.  Since as you mention the i.MX6 has overvoltage protection.  I do not have the parameter of how much it is the maxim to allow but in this case it is cleary less than the 3.3v that supports this pad.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,341 次查看
keitanagashima
Senior Contributor I

Hi jamesbone,

Hello. Sorry, I have additional questions.

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

[Q2]

Is there limitation on the time of voltage applied?

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

Best Regards,

Keita

0 项奖励
回复
1,342 次查看
jamesbone
NXP TechSupport
NXP TechSupport

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

ANSWER: Yes, all the GPIO Type Pads had an overvoltage protection

[Q2]

Is there limitation on the time of voltage applied?

ANSWER. Yes there are but the value it is not available in our datasheet, so it is not validated, I apologize for the inconvenience.

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

ANSWER.  If you we are talking about the I2C pad, it is different from the GPIO pad, nevertheless it is in the same pin, so I do not see any problem applying the 2.0v for 20ms


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,341 次查看
keitanagashima
Senior Contributor I

Hi Jaime,

Thank you for your reply.

OK. Thank you.

Best Regards,

Keita

0 项奖励
回复