About the output impedance of Pin Pad for i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the output impedance of Pin Pad for i.MX6ULL

Jump to solution
622 Views
yuuki
Senior Contributor II

Dear all,

We investigate Drive strength/Slew rate/Speed setting of Pad of i.MX6ULL.

We refer to the following document.
<AN5078>
https://www.nxp.com/docs/en/application-note/AN5078.pdf
 - Table 7. Influence of slew rate and output impedance (P.14)

A parameter of Drive strength and Slew rate is listed in this Table.
However, the Speed setting is not included.

Is there Table which added Speed parameter to Table7?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Solution
493 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Yuki,

>>Is there Table which added Speed parameter to Table7?

   No, there is not.

For PAD's driver strength seting, each pad can be configured, for example "SNVS_TAMPER9" PAD, see reference mauanl, page 1521:  IOMUXC_SNVS_SW_PAD_CTL_PAD_SNVS_TAMPER9 field descriptions


Have a great day,
TIC Weidong Sun
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
494 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Yuki,

>>Is there Table which added Speed parameter to Table7?

   No, there is not.

For PAD's driver strength seting, each pad can be configured, for example "SNVS_TAMPER9" PAD, see reference mauanl, page 1521:  IOMUXC_SNVS_SW_PAD_CTL_PAD_SNVS_TAMPER9 field descriptions


Have a great day,
TIC Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos