About the modification of UART1 pins used in DDR-Stress-tester for i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the modification of UART1 pins used in DDR-Stress-tester for i.MX6DL

Jump to solution
1,320 Views
yuuki
Senior Contributor II

Dear all,

We want to run DDR Stress Tester on the our original iMX6DL board.
However, in our board, USB_OTG is not implemented.
And, SD3_DAT6/ALT1(RX) and SD3_DAT7/ALT1(TX) are used as UART1.

DDR_Stress_Tester_V1.0.2_UART1_for_SDboot&JTAG.zip uses CSI0_DAT10/ALT3 and CSI0_DAT11/ALT3 as UART1.
It is necessary for us to modify it to use following pins of UART1.
- RX:SD3_DAT6/ALT1
- TX:SD3_DAT7/ALT1

Therefore, I got a source code of the DDR_Stress_Tester_V1.0.2.zip from FSL local FAE.

For UART1 pins, we made the following modifications.

iMX6_DDR_Stress_Tester_source\src\mx6dlのhardware.c

[Before]
#elif UART1_1
    /* UART1 TXD */
    writel(ALT3, IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT10);
    /* UART1 RXD */
    writel(ALT3, IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT11);
    // daisy chain setup
    writel(0x1, IOMUXC_UART1_IPP_UART_RXD_MUX_SELECT_INPUT);

[After]
#elif UART1_1
    /* UART1 TXD */
    writel(ALT1, IOMUXC_SW_MUX_CTL_PAD_SD3_DAT7);
    /* UART1 RXD */
    writel(ALT1, IOMUXC_SW_MUX_CTL_PAD_SD3_DAT6);
    // daisy chain setup
    writel(0x11, IOMUXC_UART1_IPP_UART_RXD_MUX_SELECT_INPUT);

DDR_Stress_Tester_V1.0.2.zip uses USB_OTG port.
It is necessary for us to switch from USBOTG to UART1.

Would you teach a modification file and the contents to change from USB_OTG to UART1?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please enter service request, I will send it to you.

Best regards

igor

View solution in original post

0 Kudos
Reply
8 Replies
883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please follow recommendation on link below in case when USB_OTG is not available:

If  USB OTG port is not available on customer board, please use the images in

DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG.zip.

The bin files in the packages can be loaded by uboot and elf files are used by JTAG load.

i.MX6 DDR Stress Test Tool V1.0.3

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
883 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your quick response.

The DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG image uses CSI0_DAT10 pin and CSI0_DAT11 pin for UART1.

In customer board, UART1 is assigned SD3_DAT7 pin and SD3_DAT6 pin.
Therefore we cannot use DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG.

It is necessary for us to modify a source code of DDR_Stress_Tester_V1 .0.2.

We understood the method to set pins of UART1.
However, we do not understand a method to change from USB-OTG to UART1.

Would you teach this method?

Or, would you send it to me if there is a source code of DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG?

Best Regards,
Yuuki

0 Kudos
Reply
883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

there is no "method to change from USB-OTG to UART1"

since iROM uses SDP for loading image - it uses only USB OTG,

it can not be changed to UART: this is hardware limitation.

So one needs to use JTAG.

Best regards

igor

0 Kudos
Reply
883 Views
yuuki
Senior Contributor II

Dear Igor-san.

Thank you for your response.

I suppose that DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG binary image is made by DDR_Stress_Tester_V1 .0.3 source code.

Would you teach the change point when DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG was made?

Best Regards,
Yuuki

0 Kudos
Reply
883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

there are no changes, just follow "MX6_DRAM_Stress_Test_Guide_vx.pdf"

whch is included in DDR_Stress_Tester package p.12:

..This creates the DRAM Stress Test images (.bin and .elf files) under the directory

.\dram_stress_test\output\mx6x\bin (Note that a new directory .\dram_stress_test\output has been created)

6. The .elf file can be used with a JTAG debugger

also please follow this document sect.5 How to run the DRAM Stress Test from the debugger

Best regards

igor

0 Kudos
Reply
883 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

I do not have MX6_DRAM_Stress_Test_Guide_vx.pdf document.
Can you send this to me?

Best Regards,

Yuuki

0 Kudos
Reply
884 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please enter service request, I will send it to you.

Best regards

igor

0 Kudos
Reply
883 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for yoru support.

I made the following SR.

1-3694444541

Would you respond about this?

Best Regards,

Yuuki

0 Kudos
Reply