About the ability to run custom applications without using an external ROM on i. MX6 Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the ability to run custom applications without using an external ROM on i. MX6 Solo

Jump to solution
1,047 Views
azausatu
Contributor I

Hello!

I use a processor i.MX 6 Solo. I want to run my applications without using external RAM and ROM memory, without operating systems, bare metal.

Questions:
1) does the processor have internal ROM memory for storing user applications?
2) If the application can be loaded into internal permanent memory, please give information on how to do this. Use mfgtool? How do I configure booting from internal memory?
3) i.MX 6 Solo can only be used with external permanent memory?


Thank you very much!
I apologize for the stupid questions.

Labels (2)
0 Kudos
Reply
1 Solution
930 Views
kunalkotecha1
Senior Contributor II

Hi Azamat G.,

I believe internal ROM is the Read-Only Memory and won't be able to use the same for flashing an application. Below is the screenshot of available boot devices. Please refer to section 8.5 of the attached Reference Manual for further details.

pastedImage_1.png

Let us know if you have any further queries on the same.

Regards,

Kunal

View solution in original post

1 Reply
931 Views
kunalkotecha1
Senior Contributor II

Hi Azamat G.,

I believe internal ROM is the Read-Only Memory and won't be able to use the same for flashing an application. Below is the screenshot of available boot devices. Please refer to section 8.5 of the attached Reference Manual for further details.

pastedImage_1.png

Let us know if you have any further queries on the same.

Regards,

Kunal